Murrelektronik

Automation

Oct 01, 2016

Installation as easy as closing the handle

Connecting machine components is easier now with the Modlink Vario Square, Murrelektronik's practical media coupler in rectangular format. Connect and disconnect pneumatic, fluid and power, also under pressure, reliably and without a drip.

The media coupler is ideal especially in machines and plants where connections between components and controls cabinets, machine components, or tools are subject to frequent switching. The user-friendly Modlink Vario Square quick-locking system is also cost-efficient. The handle, which is also used to bundle cables, can be locked in five different positions – whatever is needed for the application.

Modlink Vario Square has space for eight slots, which can be used for pneumatics, fluid and power as required. It’s a module that enables modular machines and installations. Murrelektronik offers all the accessories with various pinning and encoded M12 lines. Thanks to solid metal housing, the Modlink Vario Square is ready for rugged industrial conditions.